Other Parts Discussed in Thread: CC3200, CC2650
Hi,
After playing with the cc2650 in both sensortag and launchpad variants I had a client request I do some customisation to the wifi sensortag counterpart as the base for a proof of concept. I ordered a couple of cc3200 sensortags (as that is the device the client hopes to use for demos). I assumed things would be as simple and straightforward as TI has gotten me used to, so I even ignored the "For Wi-Fi development and prototyping, TI recommends the CC3220SF LaunchPad development kit featuring the CC3220SF wireless MCU." warning on the order page.
Receiving the sensortags, I tried to find the source code for the original firmware (so I can recover from mistakes) and some sdk to work with, and was kind of surprised to see that others have asked, and the answer is that it is not yet available as the device has not officially launched, whatever that means:
- https://e2e.ti.com/support/wireless_connectivity/simplelink_wifi_cc31xx_cc32xx/f/968/t/618754
So I'm at a loss here... Is it still the case that TI will not provide a way to develop custom firmware for the cc3200 sensortag? Will this stay the case forever?
Thanks