Hello,
As far as I understand, CC3220, like the CC3200 does not support NDK, because it also has its own
TCP/IP Stack in NWP. Is it possible to organize PPP-exchange by the serial line with the 3G-modem
(requires support for LCP + PAP/CHAP with md5 + IPCP + IP) for the CC3220 with its built-in protocol stack?
If this is possible, which version of R/S/SF is more suitable for this purpose?
If the CC3220 stack does not contain PPP also, then is it possible to replace the CC3200 with another
similar model for this purpose?