Part Number: WL1807MOD
Tool/software: Linux
Hi Champs,
Have you realized more than 3km commutation on the WL18xx series ?
According to customer investigation, this is possible to realize with external directive antenna.
If you have such a parameter or sample code , could you please tell ?
Actually, customer tried to more than 3km communication. However, they failed communication between AP and STA connection.
When they scan SSID at this AP and STA with 3km, SSID scan is able to confirm between AP and STA.
Then, RRSI show Rx sensitivity around -80dBm. So, RF performance has affordable.
They also confirmed SSID information at 5km. So, RF signal quality and noise must be no problem.
When they look into log and packet capture, AP side send Association Response. On the other hand STA side didn't sent ACK.
After this STA send data flame that is created by MAC address exchange , it disconnected due to "Class 3 frame received from nonassociated STA"
However, they confirmed when we established AP and STA connection near distance.
Then , they moved to 5km point this data flame communication is continue available.
We used to previous thread about "ACK Timeout" issue. However, we suspect another issue due to above additional information.
So, could you advice some suspect register or code ?
Regards,
Kz777