Hii
Can anyone share any example or project for CC3100 driver for stm32f4 with noOS for hal drivers with the given SDK stm32 example i am not able to work
Thanks
Jagath
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hii
Can anyone share any example or project for CC3100 driver for stm32f4 with noOS for hal drivers with the given SDK stm32 example i am not able to work
Thanks
Jagath
Part Number: CC3100
hii
i am getting error of
Error[Pe059]: function call is not allowed in a constant expression E:\ti\workspace\iar\cc3100Stm32F4\Src\wi-fi\simplelink\include\wlan.h 598
at #if _SL_INCLUDE_FUNC(sl_WlanDisconnect)
and
Error[Pe020]: identifier "SlDeviceEvent_t" is undefined E:\ti\workspace\iar\cc3100Stm32F4\Src\wi-fi\WiFiMgr.h 17
where i am gone wrong
Thank you
Jagath
Hi Jagath,
Did you copy the Drivers folder to the CC3100 SDK? The STM32 bring-up guide is in the docs/examples folder of the SDK: http://processors.wiki.ti.com/index.php/CC3100_%26_STM32F4_Bringup_Guide
I verified both stm32discovery projects provided in the SDK should compile.
Best regards,
Sarah
Part Number: CC3100
hii
i am trying to configure cc3100 to ap mode host is stm32 (Non os) and the board is custom board but i followed the procedure simplelink stm32 example but it is stuck in this loop
if (ROLE_AP == mode)
{
/* If the device is in AP mode, we need to wait for this event before doing anything */
while(!IS_IP_ACQUIRED(g_Status)) { _SlNonOsMainLoopTask(); }
}
thank you
Jagath
Hi Jagath,
Are you running the getting_started_with_wlan_ap example from the SDK? Do you have the latest servicepack flashed? Please see: http://processors.wiki.ti.com/index.php/CC3100_%26_CC3200_UniFlash_Quick_Start_Guide#Service_Pack_Programing
Best regards,
Sarah
hii sarah
i am using spi communication.
STM32 and cc3100 custom board
it is getting out of this loop present in configureSimpleLinkToDefaultState()
if (ROLE_AP == mode)
{
/* If the device is in AP mode, we need to wait for this event before doing anything */
while(!IS_IP_ACQUIRED(g_Status)) { _SlNonOsMainLoopTask(); }
}
Thank you
Jagath
Hi Jagath,
Best regards,
Sarah
hii Sarah
i am using stm32f446z as the controller. The example is from cc3100 sdk 1.3.0 stm32f4 discovery ap example. i am stuck in
if (ROLE_STA != mode)
{
if (ROLE_AP == mode)
{
/* If the device is in AP mode, we need to wait for this event before doing anything */
while(!IS_IP_ACQUIRED(g_Status)) { _SlNonOsMainLoopTask(); }
}
inside configureSimpleLinkToDefaultState() function and uart shows [general event]
i have not flashed the latest service pack.
With the same setup and with freeRtos i can able to drive the cc3100 in AP and STA mode but without FreeRtos i am not able get..
Thank you
Jagath
Hi Jagath,
Have you made any changes to the getting_started_with_wlan_ap example or to the Wi-Fi host driver?
What changes have you made to run this example with FreeRTOS?
Best regards,
Sarah