This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3235MODSF: Can I customize response data from 'at_commands' example?

Part Number: CC3235MODSF
Other Parts Discussed in Thread: CC3235SF

Hello,

I'm using a CC3235MODSF and a main MCU for my product.

Those are communicate with at commands by UART based on the 'at_commands' example.

I am struggling with response data to send to main MCU.

For example,

If the main MCU sends "at+start" command to the CC3235MODSF,

CC3235MODSF responds "at+start\nOK\n\r" to the main MCU and then sends additional data like "+eventwlan:~~~~~~~~".

It makes me hard to getting and parsing the response data in the main MCU firmware.

I want to make the CC3235MODSF sends only 1 response data for the 1 request.

For example, "at+start\nOK\n+eventwlan:~~~~~~~~\n\r".

Where can I customize the response data from the 'at_commands' example?

Thanks,

Calvin