This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3235S: the full duplex feature in the 802.11 n WiFi standard supported by the board

Part Number: CC3235S


I want to make 2 CC3235S boards communicate with each others using WiFi P2P mode and I succeeded in this, my question now is one of the standards that are supported in CC3235S is 802.11 n which has a full-duplex feature, so how can I configure the WiFi to use this specific standard, not the other supported ones?