Part Number: BOOSTXL-CC3135
Other Parts Discussed in Thread: CC3100, CC3100SDK, CC3135
Hi E2E,
I am testing BOOSTXL-CC3135 connected with STM32F4-Discovery.
Hardware : STM32F4 Discovery board + BOOSTXL-CC3135 and CC31XXEMUBOOST
Software : STM32F4_Add_On_for_CC3100_SDK
Followed the steps in CC31xx & STM32F4 Bringup Guide.pdf(provided in the SDK, unfortunately, the link http://processors.wiki.ti.com/index.php/CC31xx_%26_STM32F4_Bringup_Guide has lost. I attached the PDF below), there're some questions I want to ask.
cc3100_stm32f4_discovery_guide.pdf
The following figure is a partial screenshot of the PDF:
1. As the PDF said in step 6 above, I didn't find the sl_common.h document in the example project folder(D:\TI\CC3100SDK_1.3.0\cc3100-sdk\platform\stm32discovery\example_project_iar\getting_started_with_wlan_station). Where can I find it?
2. In step 8 above, the application details links of these two examples have lost too. So, are there any other links or documents I can get to see the application details?
Regards,
Siemin