Part Number: CC2538
Other Parts Discussed in Thread: Z-STACK, Z-STACK-ARCHIVE, CC2530
Hello E2E community,
I am working on CC2538 Zigbee Z-stack Embedded firmware.
I am trying to send the Write Attribute command from Zigbee Linux Gateway Application 3.0 to a CC2538 Device.
If I am sending a write attribute command to a device & It was sent successfully over the network.
Device is immediately Responding it with status as SUCCESS.
But on the Gateway Application side, I am not able to receive any kind of indication or response related to it.
After predefined timer interval it will invoke the time out condition.
i.e.
I am not getting why this is happening. so I go through logs on gateway application & sniffer data.
& found that my gateway application little bit slower than the hardware device. (i.e. CC2538 router/end device).
Will you please help to solve this problem....
1. how I put some response time delay for the each incoming request?...
2. is there any another way to handle this condition?...
NOTE : Find the attachment given below for sniffer data & Zigbee logs.
Thanks & Regard's
Shiv Patil.