Part Number: CC1352P
Other Parts Discussed in Thread: ENERGYTRACE, LAUNCHXL-CC26X2R1
SDK Version: 5.10
HW: Launchpad
We use OOB zed_sw_ota_client and bim_offchip projects, and the power consumption is about 1mA when the device sleeps.
After we changed the LF XOSC in the CCFG to LF RCOSC, the sleep power consumption did not change.
Q1. How to solve this problem?
Q2. We also face the same problem in the SimpleLink CC13x2/26x2 SDK Zigbee on chip OAD project. Is the solution the same?