Part Number: CC2652P7
Other Parts Discussed in Thread: SYSBIOS
Is it OK to call task_construct after Bios_Start? Will the task be able to run with the expected priority?
BR,
Shuyang
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Shuyang,
Tasks can be created and deleted dynamically, please see Section 3.6 of the SYS/BIOS (TI-RTOS Kernel) User's Guide.
Regards,
Ryan
Thanks Ryan.
I have one more question: either task_construct and task_create can be used dynamically right? What’s the difference between these two apis?
BR,
Shuyang
The create APIs require a heap to allow dynamic memory allocation of the object. The construct APIs must be passed an object structure instead of dynamically allocating the object from a heap, helping reduce the code footprint. This can also be seen in the ti.sysbios.knl.Task module of the TI-RTOS Runtime Kernel APIs.
Regards,
Ryan