Part Number: LP-CC2652RSIP
Other Parts Discussed in Thread: CODECOMPOSER, CC2652RSIP, SIMPLELINK-CC13XX-CC26XX-SDK,
Hi, TI Support Team! This question relates to the UART usage of the board.
I flashed the board with UART ZNP and trying to work with it through the Hardware UART D12, D13 PIO. And run into directly the same issue as mentioned here.
It doesn't matter whether the board is powered from the Debugger or from the external power source (yes, I have changed the jumper position).
I can add that the ZNP Doen't work with the UART-USB sticks like cp2103 and all the others (when it's connected to the Hardware UART).
The only time when I can get it working - is when I use the /dev/ttyACM0 formed by the native board debugger (and jumpers are in the relative postions, ofcourse).
it doesn't matter whether I an trying to use our proprietary SW or the native TI zigbeeHaGw script to run the servers.
Please, help me to understand what can be the issue.
ZNP SRC (CodeComposer) in attachment.
Please, note: UART WORKS! but EXTREMELY Unstable. I can start the znp using UART-to-UART connection only 1 time to 5.
The Hardware on the "Host" (where zigbeeHAgw and servers are located) doesn't matter - it doesn't work on:
Orange Pi, Raspberry PI, our custom Mediatek Board, USB-UART stick connected to the host PC, etc...
Settings are the same as in the ZNP config.
znp_LP_CC2652RSIP_tirtos_ccs.zip