Other Parts Discussed in Thread: TS3USB31
Hi, TI support team.
I already asked this issue with previous post, but I would like to ask you again.
We are concerning with USB signal voltage would be added to CC2531 DP/DM pin in spite of CPU is power down.
Our system is powered on by mechanical switch, therefore there will be a state the USB is connected but CPU is power off.
I guess it seems OK during the USB Host doesn't detect DP pull up voltage from USB peripheral like this CC2531 system.
My understanding is, after CC2531 system power on, the USB host start to drive DP DM line to connection.


USB connected and VBUS rises to 5V. CPU Vdd3.0V is power off until the switch will be turned ON.
But to protect CPU pin over voltage, I would like to add TS3USB31 USB
bus switch for CPU protection.

Could you tell me Is this measure needed for this matter ?
I guess this countermeasure is too complicated.
How about is this issue do you think ?
Your help is highly appreciated.
Best regards,
Yoshiaki Maehara