Part Number: CC2652P
Other Parts Discussed in Thread: CC1352P,
Hi,
I am using launch pad CC26X2R1_LAUNCHXL to external target as CC2652P1F, I don't know which file is used to examples for CC2652P1F. please guide me how to choose the SDK File.

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I build the project and done flash the CC2652P1F but devices are not added and controlled i could not find the error
I build the project in ccs then extract hex file from the project i use the hex file to flash the CC2652P1F
Which example do you build and run? Do you revise example according to your own schematics?
If you use ZNP, you need to use another host application such as ZTool to run application. Do you use ZTool or other host application when you test ZNP?
I tested on my own application and I run the coordinator to start as network but modules would not pair with coordinator
Does your application and ZNP act as coordinator? If so, do you enable permit join on your coordinator?
What is your device to join network? Are you sure the device sends beacon request to scan and join network?
Hi Praveen,
I was under the impression that you had a working setup (at least starting up the Zigbee network with a CC2652P ZNP) last week, so there must be a separate issue with your application (i.e. not Z-Tool) which is causing the problem. Have you made any hardware changes since your last E2E thread?
Regards,
Ryan
Make sure you factory reset the device or erase all memory and re-program before attempting to start up the revised firmware and form a new network.
Regards,
Ryan