Part Number: CC2652P7
Other Parts Discussed in Thread: CC2652P, CC2530, CC2591
Hi team,
Here's the request from the customer:
Application Scenario: Using CC2651P/CC2652P without paying attention to power consumption, ZC+ZR scheme, no zed. In the later stage, customer will consider switching the ZR to a BLE device by OTA.
Because of the urgent project and material delivery time is limited, there is two plan submitted by customer:
- Completely based on TI's solution, using internal PA scheme.
- Based on the experience of CC2530, external PA scheme. (Hope to keep the software unchanged and compatible with the internal PA scheme)
The radio frequency part is as follows:

Is the logic of DIO28/29 controlling RF SWITCH the same as the previous control logic of CC2591?
Could you help check this case? Thanks.
Best Regards,
Nick