This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2652P: Latencies and pairing troubles in an open field straight line application with 19 devices

Part Number: CC2652P


Good morning.

We are testing a custom application involving some custom firmware based on zr_genericapp and zed_genericapp, our last setup was represented by the following topology:

In which there are 14 custom ZEDs, 3 custom ZRs and 1 default ZR, each router is spaced out around 40 meters in a straight line from the others, while the end devices are placed in the path between the routers.

Each device is set to transmit at 20dBm, and we are using some dipole ipex antennas in an almost rural area.

The custom devices contains 8 endpoints of type Smart Plug.

My goal is to measure the poll time of each metering measure of each endpoint (currentSummDelivered of cluster seMetering).

The problems i have found are mainly the following:

  1.  I paired all the devices in my lab, so the end-devices have paired to some parents in a temporary way differently then the final topology, thinking that they would change parents in field finding the best ones: and this correctly happened just for 7-8 of the ZEDs, the remaining ones finally resulted to be disconnected in the networkmap. So i had to walk to the disconnected ones in order to reset and re-pair them, which resulted in the correct final topology. What am i missing? I have avoided the in-field pairing because tipically it requires a variable number of retries (factory reset and pair button press) as almost never the pairing and interview go well at the first attempt, while in lab (on desktop), they always complete successfully.
  2. As i have the desired topology, i run a script of mine in order to poll each device endpoint (8 for each device) for its 2 cluster attributes of my interest, which are currentSummDelivered and OnOff: the latencies that i'm experiencing are not very good, the needed time to get the full meters/onOff is around 1m 33s polling for 8 endpoints, and 24s polling for 1 endpoint (See log).

Field test, top 5, 3 routers, 14 end devices, 1 endpoint polled for each device
////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////
Device: 0x00124b0025906ff3 [Router],            Time elapsed: 104.0501ms, Average per attribute : 52.02505ms
Device: 0x00124b00259087a1 [EndDevice],         Time elapsed: 111.1384ms, Average per attribute : 55.5692ms
Device: 0x00124b0025908a6a [EndDevice],         Time elapsed: 110.2387ms, Average per attribute : 55.11935ms
Device: 0x00124b0025907cb1 [EndDevice],         Timed out
Device: 0x00124b002590e021 [Router],            Time elapsed: 794.8357ms, Average per attribute : 397.41785ms
Device: 0x00124b002590dd33 [Router],            Timed out
Device: 0x00124b002590e188 [EndDevice],         Timed out
Device: 0x00124b0025910009 [EndDevice],         Time elapsed: 132.7311ms, Average per attribute : 66.36555ms
Device: 0x00124b0025907b5c [EndDevice],         Time elapsed: 435.9508ms, Average per attribute : 217.9754ms
Device: 0x00124b0025908a25 [EndDevice],         Time elapsed: 319.9962ms, Average per attribute : 159.9981ms
Device: 0x00124b002590f613 [EndDevice],         Time elapsed: 381.8213ms, Average per attribute : 190.91065ms
Device: 0x00124b0025909133 [EndDevice],         Time elapsed: 282.9713ms, Average per attribute : 141.48565ms
Device: 0x00124b0025907b63 [EndDevice],         Time elapsed: 151.1411ms, Average per attribute : 75.57055ms
Device: 0x00124b002591071d [EndDevice],         Time elapsed: 157.2716ms, Average per attribute : 78.6358ms
Device: 0x00124b002590e1d0 [EndDevice],         Timed out
Device: 0x00124b002590dd78 [EndDevice],         Time elapsed: 645.0995ms, Average per attribute : 322.54975ms
Device: 0x00124b002590fbf6 [EndDevice],         Time elapsed: 467.6726ms, Average per attribute : 233.8363ms
Full poll time: 23.9009177s
////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////

Field test, top 5, 3 routers, 14 end devices, 8 endpoints polled for each device
////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////
Device: 0x00124b0025907b63 [EndDevice],         Time elapsed: 1.4851941s, Average per attribute : 92.824624ms
Device: 0x00124b0025910009 [EndDevice],         Time elapsed: 785.6044ms, Average per attribute : 49.100267ms
Device: 0x00124b002590e021 [Router],            Time elapsed: 3.1569569s, Average per attribute : 197.3098ms
Device: 0x00124b0025908a6a [EndDevice],         Time elapsed: 1.4947743s, Average per attribute : 93.423387ms
Device: 0x00124b0025909133 [EndDevice],         Time elapsed: 3.2124645s, Average per attribute : 200.779026ms
Device: 0x00124b002590e1d0 [EndDevice],         Time elapsed: 1.8394391s, Average per attribute : 114.964936ms
Device: 0x00124b0025906ff3 [Router],            Time elapsed: 3.4791768s, Average per attribute : 217.448546ms
Device: 0x00124b002590dd33 [Router],            Timed out
Device: 0x00124b0025908a25 [EndDevice],         Time elapsed: 1.5380671s, Average per attribute : 96.129187ms
Device: 0x00124b002590dd78 [EndDevice],         Time elapsed: 2.8397282s, Average per attribute : 177.483006ms
Device: 0x00124b0025907cb1 [EndDevice],         Timed out
Device: 0x00124b002590fbf6 [EndDevice],         Timed out
Device: 0x00124b00259087a1 [EndDevice],         Time elapsed: 1.0135207s, Average per attribute : 63.345037ms
Device: 0x00124b002591071d [EndDevice],         Time elapsed: 703.0589ms, Average per attribute : 43.941175ms
Device: 0x00124b002590f613 [EndDevice],         Time elapsed: 1.1584657s, Average per attribute : 72.4041ms
Device: 0x00124b002590e188 [EndDevice],         Time elapsed: 1.8645467s, Average per attribute : 116.534165ms
Device: 0x00124b0025907b5c [EndDevice],         Time elapsed: 2.1748023s, Average per attribute : 135.925138ms
Full poll time: 1m33.2618987s
////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////

So, in this test, the devices with smart plug endpoints were just 17 (3 custom routers + 14 custom end-devices), but we would like to make a single coordinator handle around 200 of them, carefully partitioned in routers and end-devices, in order to avoid the require of too many router-router hops (wich we experimented to be limited to 10).

In other words, we would like to take the topology in picture, raise the device number to 30, and make it like a brench of a star centered in the coordinator and having, for example, 6 of those branches.

How can it scale? Can we hope to poll the full metering and onOff attributes of each endpoint of each device in a time falling in the ten of minutes? And for the actuation, can we expect to command an ''On'' or ''Off'' command in a reliable way having it previous and next state confirmed in a time below a second?

Is this kind of application really suitable to be done with the Zigbee protocol? Or maybe we have to evaluate some WiFi modules? Replacing the coordinator with an access point,  zigbee routers with WiFi repeaters and end-devices with client nodes.

Any advice will be very appreciated.

Thank you again for the extremely ready and prepared support.

Roberto

  • Hello Roberto,

    1. Please review Unsecured Join to a Centralized Network.  Per default of the zd_app.c, End Devices will try to securely rejoin the same network BDB_MAX_SECURE_REJOIN_ATTEMPTS times before trying unsecure/trust center rejoins.  If MAX_RESUME_RETRY is eclipsed or TC rejoins fail then the device will attempt a normal join, which required the network to be open for joining from routing nodes.  Also, if the Trust Center does not authenticate the device after a TC rejoin by MAX_DEVICE_UNAUTH_TIMEOUT then the device will be factory reset.  You can modify zd_app.c to change this behavior, as in these E2E thread examples:

    https://e2e.ti.com/f/1/t/1163283 
    https://e2e.ti.com/f/1/t/1176456 

    2. We have already discussed latency and sleepy ZED polling versus always-on from your previous E2E threads.  It should be possible to poll for attributes within less than 10 minutes, especially if using groups or broadcasts.  There is also automatic attribute reporting available, has this already been considered?  You could have multiple Zigbee networks where the ZC is a gateway which reports to and receives commands from a common Cloud service, such that it appears to be on congruous Zigbee network.  It is still possible to have a Zigbee network with 200 nodes without the Cloud/gateway option, however creating specific device associations (if desired) will be a challenge.

    Regards,
    Ryan

  • Hello Ryan

    Thank you, i'm going to try the end-device rejoin behaviour setting BDB_ATTEMPT_UNSECURE_REJOIN to false (default is true) and BDB_MAX_SECURE_REJOIN_ATTEMPTS  to 255 (default 3).

    About the second point, i have set the end-devices as always-on, so the time required to poll one of their cluster attribute by the Zigbee2Mqtt istance is comparable with the time required for the routers, between 50 to 100 ms, so the full polling of around 20 devices require almost 2 minutes, do you think this is the minimum latency reachable in your opinion?

    The auto attribute reporting seems not optimal for our topologies thinking about semi-straight line of routers and end-devices. Or is it?

  • If I understand it correctly, 20 devices each have 8 endpoints with 2 attributes so you would be sending 320 read requests which will trigger the same amount of read responses.  If each request/response bidirectional communication took 400 ms to complete (assuming some retries would be necessary) then this would amount to about 2 minutes total.  SWRA650 demonstrates less latency for a larger network.  Since attribute reporting is unidirectional, this reduces the end-to-end packet completion distance and total number of packets necessary.  It also lowers the strain on the ZC having to send out so many messages.  You could create a timer to keep track of which end devices have reported and whether any are missing.

    Regards,
    Ryan