Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1352P: Build errors after Custom Board in proyects for launch pad

Part Number: CC1352P
Other Parts Discussed in Thread: SYSCONFIG

Hi TI!

I need to customize the zc_generic project. This project is closed for Launch Pad.

To customize the project I select the "Show Board View" option in SysConfig and choose "Use Custom Board". But then when I try to compile I get 2 build errors.

I show them in the attached image.


I am using sdk 6_30 and CCs12.1.0

The error seems to be with the output .out file.

How can I solve these errors?

Thank you very much.