Part Number: CC2652P7
In continuation to the question linked above,
I am not able to get LFB182G45BGEF296 part from Murata website.
Please let me whether you got this part from Murata or any other new part from other manufacturer.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CC2652P7
In continuation to the question linked above,
I am not able to get LFB182G45BGEF296 part from Murata website.
Please let me whether you got this part from Murata or any other new part from other manufacturer.
Hi Ryan,
This SWRA629 reference design is for 2.4GHz regular port and sub GHz port.
Can this be used for High Power PA(+10dBm Tx Port)?
I am referring to SWRA729 and SWRA640g application reference notes.
Please refer to the below table for High Power port SWRA640g Page28/39..

Please clarify me if i am wrong.
Thanks
Suresh
9789010168
Please be patient as the SimpleLink hardware experts are on leave until January 3rd. I believe that either balun can be used, however you could contact Murata for further clarification and additional recommendations.
Regards,
Ryan
Hi Suresh,
As noted in the previous thread the Murata website is not always updated with all their available devices. Please contact Murata sales directly (i.e. phone or email) to request the part.
Jake
Hi Jake,
I contacted Murata. They have this part. I got the datasheet along with the samples required for Proto.
Thanks
Suresh