Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2531: USB module is not currently being used

Part Number: CC2531

Hi Experts,

Our customer has a question about the CC2531.

If the USB module is not currently being used, can the VUSB be left Open or must it be tied to +3.3V?

Also, if Vusb does not have to be tied to +3.3, should it be pulled down through a resistor?

We saw this E2E post below:
(+) CC2531 - unused USB - Other wireless technologies forum - Other wireless - TI E2E support forums

In this thread the user asks if it is OK to ground all of the USB pins (including the DVDD_USB pin), not leave it open.   As a matter of fact, it raises the question of whether or not the USB_P, USB_N, as well as the DVDD_USB  pins can be left unconnected?

 We hope to receive your confirmation. Thank you.

Best regards,
Gerald