Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1352P: Z-stack ZNP and MT Interface for CC1352P

Part Number: CC1352P
Other Parts Discussed in Thread: Z-STACK

Hello everybody

I Have three  questions  with z-stack for CC1352P

 

1.Is it possible to perform zigbee communication on 915 MHz frequencies, or it only allows to perform zigbee communication on 2.4 GHz?

2.Can I change the frequency to 915 MHz through the MT commands or ZNP to perform zigbee communication, which are in the "Z-Stack Monitor and Test API" document?

3.In case it is possible to perform zigbee communication on 915 MHz in MT commands or ZNP, could you please provide me an example. ?

Thank you and best regards!