Part Number: CC2531
Other Parts Discussed in Thread: , PACKET-SNIFFER
Hello everyone.
It is not my habit to be posting on forums but I've been stuck on the problem for days.
I have two CC2531EMK dongles that I am using for Zigbee testing. Both are flashed with sniffer_fw_cc2531.hex firmware (successfully as they work just fine alone) using cc-debgger,
My trouble is that while both dongles are recognized by pc:
└─$ lsusb
Bus 002 Device 036: ID 0451:16ae Texas Instruments, Inc. CC2531 Dongle
Bus 002 Device 034: ID 0451:16ae Texas Instruments, Inc. CC2531 Dongle
└─$ lsmod | grep cdc_acm
cdc_acm 45056 0
usbcore 344064 7 usbserial,ohci_hcd,ehci_pci,usbhid,cdc_acm,ehci_hcd,ohci_pci
Premissions dialout to user are set.
None of them is listed in /dev/tty* as ACM0 or ACM1 - I had to add those manually.
I am trying to run different tools where without specifying any device, they run just fine, but don't run at all if I try to specify device as /dev/ttyACM0 as they are not found.
I tried flashing one CC2531 dongle with another firmware (to try to differentiate them) but the ONLY successful firmware is the one listed above (be from public sources or from here - doesn't matter).
I am quite new to zigbee and similar but I'd greatly appreciate any support as I've been stuck here for awhile, emptied all of my resources that I found.
Both dongles are plugged in and work, tried switching ports and what not.
Example of running tool:
└─$ sudo zbwireshark -c 20
zbwireshark: listening on 'CC2531 USB Dongle', channel 20, page 0 (2450.0 MHz), link-type DLT_IEEE802_15_4, capture size 127 bytes
Wireshark exited (0)
8 packets captured
Example of specifying device:
└─$ sudo zbwireshark -c 20 -i /dev/ttyACM0
[redacted]Serial issue in kbutils.isgoodfetccspi: [Errno 6] could not open port /dev/ttyACM0: [Errno 6] No such device or address: '/dev/ttyACM0'.
It'd not be a tool problem as I troubleshooted with multiple other tools, scripts etc..
I greatly appreciate any help.