This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2652P7: hardware interface help

Part Number: CC2652P7

Hi,

Designed a custom board( CC2652P7 chips -> 1 master and  3 slaves interfaces with SPI).

Unfortunately, SPI Controller and Peripheral projects in SDK are not working fine.

Only 2 of the slave's responded but not consistent. One of the slave's never responded

DIO_12 is chip select pin ( output of SPI controller, output strength configured to medium in syscfg)

DIO_13 is SPI peripheral ready pin ( which is an input to the SPI controller).

On both the lines there is a pull up of 51k Ohms. Is this ok?

What else need to be cross checked?

Thanks

Karthik