Part Number: CC2652R7
Other Parts Discussed in Thread: Z-STACK,
Hello,
I am facing a quite troublesome problem with my Z-Stack based ZED : it randomly leaves the Zigbee Network after few days.
After looking for similar threads, I found several ones, but none with clear answers on the issue. The most relatable one being CC2530: ZED leaving network randomly - Zigbee & Thread forum - Zigbee & Thread - TI E2E support forums.
Basic Product Information
- ZED is a custom product based on the SimpleLink
cc13xx_cc26xx SDK 6.40.00.13 and its ZED DoorLock Example (for LP_CC2652R7).
- ZC is also a CC2652R7, straight from the SimpleLink
cc13xx_cc26xx SDK 5.40.00.40 and its ZNP Example (and Z2M as controller).
- ZED Poll Period is 6000 ms.
Initial State
- Several identical ZEDs (4 or 5) are paired successfully with the ZC.
- All ZEDs interact properly with the ZC.
- No ZR, all ZEDs are directly routed to the ZC.
- Range is not an issue.
- There is no other device paired with the ZC.
This situation will last 2 or 3 days, where :
- ZEDs will properly report some attributes.
- ZC can interact with ZEDs on demand.
Problem Symptoms
After these few days, some of the ZEDs, not all of them, will cease to communicate with the ZC :
- ZC see these ZEDs as Non-Responsive, still in network.
- ZC Logs do not show any Leave Network messages.
- ZC interactions to these ZEDs do not succeed. Interactions with the other ZEDs do succeed.
- These ZEDs will cease to report their attributes. The others still report them properly.
- These ZEDs are still alive and active, and react to manual interactions.
With some code instrumentation, i could extract some Z-Stack states for these ZEDs :
- zstack_DevState -> zstack_DevState_HOLD
- bdbCommissioningMode -> BDB_COMMISSIONING_NWK_STEERING
- bdbCommissioningStatus -> BDB_COMMISSIONING_NO_NETWORK
Which I assume being an Out Of Network state.
Here's my question : What could possibly produce such behavior ?
Most solutions or hints I could find imply a ZR, a ZED Timeout, a great amount of devices or chips from previous generation, but none apply here.
More Informations :
- What about sniffing the RF ? Sadly, this is a quite complex procedure to implement in my environment, especially if it must last several days.
- Why trying with several ZEDs at once ? Due to the randomness of the issue, I have to use several to ensure its reproduction.
- ZED Z-Stack Configuration :
zstack.deviceType = "zed";
zstack.pm.pollPeriod = 6000;
zstack.rf.txPower = "5";
zstack.rf.primaryChannels = [11,25];
zstack.network.endDeviceTimeout = 14;
zstack.advanced.routing.routeExpiryTime = 255;
Other parameters are presumably default.
- ZED Symbols/Macros :
ZCL_REPORT_CONFIGURING_DEVICE ZCL_REPORT_DESTINATION_DEVICE ZCL_READ ZCL_DISCOVER ZCL_WRITE ZCL_BASIC ZCL_IDENTIFY ZCL_DOORLOCK ZCL_SCENES ZCL_GROUPS BDB_REPORTING TIMAC_ROM_PATCH CUI_DISABLE MAX_STATUS_LINES=10 ZSTACK_SECURITY FREQ_2_4G OSAL_PORT2TIRTOS OSAL_PORT2TIRTOS_OSALMAP ZDO_API_BASIC TC_LINKKEY_JOIN NV_RESTORE NV_INIT FEATURE_NON_BEACON_MODE ZCL_STANDALONE MAX_DEVICE_TABLE_ENTRIES=50 DEVICE_FAMILY=cc26x0 DeviceFamily_CC26X2X7 TIMAC_ROM_IMAGE_BUILD NVOCMP_NVPAGES=2 TIRTOS7_SUPPORT HEAPMGR_CONFIG=0x80 HEAPMGR_SIZE=0x00
Thanks for your time. Any lead or suggestion would be greatly appreciated !