This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TI,
We have made a Matter Occupancy sensor product with CC2652R7. We have successfully tested it with Google Nest, but we are not able to connect with an AppleTV (yes, we do have the correct version ). We then tried the default TI lock app demo which also did not connect to the AppleTV.
Two questions arises:
1) Is there an interoperability issue between TI Matter projects and Apple devices?
2) This pull request seems to indicate removal of support for CC2652R7. Is that the case? Do we have to change to an x4 device?
I was hoping Matter would finally achieve the ultimate goal of connected things: Everything being interoperable and gateway-less. So far I am a bit disappointed, but not really surprised.
Cheers,
Fredrik
Hi Fredrik,
1) Is there an interoperability issue between TI Matter projects and Apple devices?
I was able to get this working with lighting-app (as recent as last month) on iPad and Apple TV. This was with the latest commit on master branch.
2) This pull request seems to indicate removal of support for CC2652R7. Is that the case? Do we have to change to an x4 device?
Correct, due to the increased flash consumption of Matter, we now recommend the CC1354/CC2674, such as here: https://github.com/project-chip/connectedhomeip/tree/master/examples/lighting-app/cc13x4_26x4
We have made a Matter Occupancy sensor product with CC2652R7. We have successfully tested it with Google Nest, but we are not able to connect with an AppleTV
We then tried the default TI lock app demo which also did not connect to the AppleTV.
Which commit are you using? If it is an older one which had supported CC2652R7, then it's possible to have gotten "too far" behind the (auto-updated?) Apple Home / Apple TV OSes.
Can you share a serial log of what you see during commissioning?
Thanks,
Toby
Hi Toby,
I was able to get this working with lighting-app (as recent as last month) on iPad and Apple TV. This was with the latest commit on master branch.
I guess you were running lighting-app on CCxxx4?
Correct, due to the increased flash consumption of Matter, we now recommend the CC1354/CC2674
Does " we recommend the CCxxx4", really mean that Matter will not be supported at all on CC2652R7 going forward? If so, there is some documentation that should be updated accordingly. CC2652R7 is still listed as Matter compatible for example here. Btw. I remember when it was deemed crazy that the BLE Stack required 100 kB in addition to code in ROM. Now we need a 1M device to run a protocol stack?
I belive we have tried v1.0-ti-branch. I colleague also mentioned trying tag v1.2.0.1.
I do not have the log from the lock-app available right now, but here is what it looks like from our app:
Fullscreen123456789101112131415161718192021OpenThread started: OKSetting OpenThread device type to MINIMAL END DEVICEInitialize ServerSubscription persistence not supportedServer initializing...Last Known Good Time: 2023-10-14T01:16:48AccessControl: initializingExamples::AccessControlDelegate::InitAccessControl: settingDefaultAclStorage: initializingDefaultAclStorage: 0 entries loadedUsing ZAP configuration...AccessControlCluster: initializingInitiating Admin Commissioning cluster.Cluster callback: 0x0000_0030Cluster callback: 0x0000_0406Cluster callback: 0x0000_0406Updating services using commissioning mode 0Failed to remove advertised services: 3Advertise commission parameter vendorID=65521 productID=32775 discriminator=3840/15 cm=0Failed to advertise extended commissionable node: 3XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXOpenThread started: OK Setting OpenThread device type to MINIMAL END DEVICE Initialize Server Subscription persistence not supported Server initializing... Last Known Good Time: 2023-10-14T01:16:48 AccessControl: initializing Examples::AccessControlDelegate::Init AccessControl: setting DefaultAclStorage: initializing DefaultAclStorage: 0 entries loaded Using ZAP configuration... AccessControlCluster: initializing Initiating Admin Commissioning cluster. Cluster callback: 0x0000_0030 Cluster callback: 0x0000_0406 Cluster callback: 0x0000_0406 Updating services using commissioning mode 0 Failed to remove advertised services: 3 Advertise commission parameter vendorID=65521 productID=32775 discriminator=3840/15 cm=0 Failed to advertise extended commissionable node: 3 Failed to finalize service update: 3 CASE Server enabling CASE session setups Joining Multicast groups Server Listening... Initialize LEDs Initialize buttons Cluster callback: 0x0000_0406 Cluster callback: 0x0000_0406 Device Configuration: Serial Number: TEST_SN Vendor Id: 65521 (0xFFF1) Product Id: 32775 (0x8007) Product Name: TEST_PRODUCT Hardware Version: 0 Setup Pin Code (0 for UNKNOWN/ERROR): 20202021 Setup Discriminator (0xFFFF for UNKNOWN/ERROR): 3840 (0xF00) Manufacturing Date: (not set) Device Type: 65535 (0xFFFF) SetupQRCode: [MT:ALG0242C00KA0648G00] Copy/paste the below URL in a browser to see the QR Code: https://project-chip.github.io/connectedhomeip/qrcode.html?data=MT%3AALG0242C00KA0648G00 Manual pairing code: [34970112332] *** Novelda Sensor ID: 0xE6EC03E6 Chip Version: 1 ***
I believe the output from the lock-app looks fairly similar, but it does not include the pairing- and QR-code.
Thanks,
Fredrik
I guess you were running lighting-app on CCxxx4?
Yes.
Does " we recommend the CCxxx4", really mean that Matter will not be supported at all on CC2652R7 going forward? If so, there is some documentation that should be updated accordingly. CC2652R7 is still listed as Matter compatible for example here. Btw. I remember when it was deemed crazy that the BLE Stack required 100 kB in addition to code in ROM. Now we need a 1M device to run a protocol stack?
Thanks for pointing that ti.com page out. We may have updates pipelined for it, I'll reach out to the web stakeholders.
I'll also ask for an official statement, but yes, to my knowledge CC2652R7 would not be a viable for single-chip Matter application.
I do not have the log from the lock-app available right now, but here is what it looks like from our app:
The logs shown here are printed at device startup. Are you able to get logs which include the commissioning process?
The logs include commissioning. In other words, nothing happens :-)
I see... we may have reduced the logs to save on code size, such as here: https://github.com/project-chip/connectedhomeip/blob/9f810445849ac06adbd63af14307664c263a99ea/examples/lighting-app/cc13x2x7_26x2x7/args.gni#L36
Probably the same logs would show up in the case of Google Home as commissioner.
Do you see any commissioning activity on the sniffer log?
I anyway guess that the only path forward is to use a 1 MB device?
Yes, due to the memory limitation on the CC2652R7.