Part Number: LAUNCHXL-CC26X2R1
Tool/software:
Good morning,
I ran some stress test using the example zc_thermostat_sink (sdk version: 3.40, 4.40 and 7.10) and the firmware does not receive or send packets after a while, receives approximately 1100 packages.
With the sdk 3.40 I received 1171 packages.
With the sdk 4.40 I received 1236 packages.
With the sdk 7.10 I received 1263 packages.
That was my test:
- 1 launchpad with the sink firmware;
- 1 launchpad with the gpd_temperaturesensor firmware.
Execute the commissioning procedure normally, after more or less 1100 A0 packages (attribute reporting) receives from the sensor, the sink does not receive or send packages anymore.
The same behavior can be seen in the capture in attached.
The first capture (error_radio) was using the sdk 3.40 and the second one was using the sdk 7.10.
Thanks,
Cristiane Bellenzier Piaia