Part Number: CC2531
Tool/software:
Since I never heard back about using an external oscillator, I have switched back to using a 32MHz crystal tied to pins 22 & 23 with loading caps. When powered, the chip always enumerates with my laptop (windows) regardless of being held in reset or not. The enumeration is "unknown USB device: device descriptor request failed." I am unable to connect to the CC2531 via the cc debugger, so the the chip should have no code loaded into it (factory fresh). When I probe onto my crystal lines, there is no clock signal, which I suspect is the problem. Any advice on what might be causing this?
Thanks.