Part Number: LP-EM-CC2340R53
Other Parts Discussed in Thread: UNIFLASH, SYSCONFIG
Tool/software:
hi Ryan
According to the standard instance of the custom door lock, steps 1 to 3 were all carried out. However, I did not see the effect of step 4. I would like to see the request log, which includes the beacon of the lock. Please help me check which step went wrong.
The coordinator used is an instance of onoff_light.
The instance code of the door lock is as follows:
/****** Application variables declarations ******/
zb_uint16_t g_dst_addr;
zb_uint8_t g_addr_mode;
zb_uint8_t g_endpoint;
zb_bool_t perform_factory_reset = ZB_FALSE;
zb_bool_t cmd_in_progress = ZB_FALSE;
/****** Application function declarations ******/
/* Handler for specific ZCL commands */
zb_uint8_t zcl_specific_cluster_cmd_handler(zb_uint8_t param);
void test_device_interface_cb(zb_uint8_t param);
void send_toggle_req(zb_uint8_t param);
void button_press_handler(zb_uint8_t param);
void send_lock_req(zb_uint8_t param, zb_uint8_t lock_or_unlock);
/****** Cluster declarations ******/
// THIS CODE REPLACES IT
/* Door Lock cluster attributes data */
zb_uint8_t g_attr_door_lock_lock_state = 0;
zb_uint8_t g_attr_door_lock_lock_type = 0;
zb_bool_t g_attr_door_lock_actuator_enabled = ZB_FALSE;
ZB_ZCL_DECLARE_DOOR_LOCK_ATTRIB_LIST(door_lock_attr_list, &g_attr_door_lock_lock_state,
&g_attr_door_lock_lock_type, &g_attr_door_lock_actuator_enabled);
/* Basic cluster attributes */
zb_uint8_t g_attr_zcl_version = ZB_ZCL_BASIC_ZCL_VERSION_DEFAULT_VALUE;
zb_uint8_t g_attr_power_source = ZB_ZCL_BASIC_POWER_SOURCE_DEFAULT_VALUE;
ZB_ZCL_DECLARE_BASIC_ATTRIB_LIST(basic_attr_list, &g_attr_zcl_version, &g_attr_power_source);
/* Identify cluster attributes */
zb_uint16_t g_attr_identify_time = ZB_ZCL_IDENTIFY_IDENTIFY_TIME_DEFAULT_VALUE;
ZB_ZCL_DECLARE_IDENTIFY_ATTRIB_LIST(identify_attr_list, &g_attr_identify_time);
/* Groups cluster attributes */
zb_uint8_t g_attr_name_support = 0;
ZB_ZCL_DECLARE_GROUPS_ATTRIB_LIST(groups_attr_list, &g_attr_name_support);
#ifdef ZB_ZCL_SUPPORT_CLUSTER_SCENES
/* Scenes cluster attributes */
zb_uint8_t g_attr_scenes_scene_count = ZB_ZCL_SCENES_SCENE_COUNT_DEFAULT_VALUE;
zb_uint8_t g_attr_scenes_current_scene = ZB_ZCL_SCENES_CURRENT_SCENE_DEFAULT_VALUE;
zb_uint16_t g_attr_scenes_current_group = ZB_ZCL_SCENES_CURRENT_GROUP_DEFAULT_VALUE;
zb_uint8_t g_attr_scenes_scene_valid = ZB_ZCL_SCENES_SCENE_VALID_DEFAULT_VALUE;
zb_uint16_t g_attr_scenes_name_support = ZB_ZCL_SCENES_NAME_SUPPORT_DEFAULT_VALUE;
ZB_ZCL_DECLARE_SCENES_ATTRIB_LIST(scenes_attr_list, &g_attr_scenes_scene_count,
&g_attr_scenes_current_scene, &g_attr_scenes_current_group,
&g_attr_scenes_scene_valid, &g_attr_scenes_name_support);
#else
zb_zcl_attr_t scenes_attr_list[] = { ZB_ZCL_NULL_ID, 0, 0, NULL };
#endif
/* Declare cluster list for the device */
ZB_HA_DECLARE_DOOR_LOCK_CLUSTER_LIST(door_lock_clusters,
door_lock_attr_list,
basic_attr_list, identify_attr_list,
groups_attr_list, scenes_attr_list);
ZB_HA_DECLARE_DOOR_LOCK_EP(door_lock_ep, ZB_OUTPUT_ENDPOINT, door_lock_clusters);
ZB_HA_DECLARE_DOOR_LOCK_CTX(device_ctx, door_lock_ep);
static zb_bool_t error_ind_handler(zb_uint8_t severity,
zb_ret_t error_code,
void *additional_info);
/* test_device_interface_cb */
case ZB_ZCL_DOOR_LOCK_LOCK_DOOR_CB_ID:
{
zb_uint8_t lock_state = ZB_ZCL_ATTR_DOOR_LOCK_LOCK_STATE_LOCKED;
uart2_printf("Lock the door");
ZVUNUSED(zb_zcl_set_attr_val(ZB_OUTPUT_ENDPOINT,
ZB_ZCL_CLUSTER_ID_DOOR_LOCK,
ZB_ZCL_CLUSTER_SERVER_ROLE,
ZB_ZCL_ATTR_DOOR_LOCK_LOCK_STATE_ID,
&lock_state,
ZB_FALSE));
zb_osif_led_on(0);
}
break;
case ZB_ZCL_DOOR_LOCK_UNLOCK_DOOR_CB_ID:
{
zb_uint8_t lock_state = ZB_ZCL_ATTR_DOOR_LOCK_LOCK_STATE_UNLOCKED;
uart2_printf("Unlock the door");
ZVUNUSED(zb_zcl_set_attr_val(ZB_OUTPUT_ENDPOINT,
ZB_ZCL_CLUSTER_ID_DOOR_LOCK,
ZB_ZCL_CLUSTER_SERVER_ROLE,
ZB_ZCL_ATTR_DOOR_LOCK_LOCK_STATE_ID,
&lock_state,
ZB_FALSE));
zb_osif_led_off(0);
}
break;
/* in button_press_handler add */
void button_press_handler(zb_uint8_t param)
{
ZVUNUSED(param);
uart2_printf("button is pressed, do nothing\r\n");
if (!param)
{
/* Button is pressed, gets buffer for outgoing command */
zb_buf_get_out_delayed(button_press_handler);
}
else
{
user_print("button_press_handler %d\r\n", param);
// send_toggle_req(param);
send_lock_req(param, ZB_ZCL_CMD_DOOR_LOCK_LOCK_ID);
#ifndef ZB_USE_BUTTONS
/* Do not have buttons in simulator - just start periodic on/off sending */
ZB_SCHEDULE_APP_ALARM(button_press_handler, 0, 7 * ZB_TIME_ONE_SECOND);
#endif
}
}
/*send lock message*/
void send_lock_req(zb_uint8_t param, zb_uint8_t lock_or_unlock)
{
zb_uint16_t addr = 0;
ZB_ASSERT(param);
if (ZB_JOINED() ) // && !cmd_in_progress
{
cmd_in_progress = ZB_TRUE;
user_print("send_lock_req %d - sending %s command\r\n", param,
"LOCK" );
/* Send Door Lock command via binding (destination unknown) */ // ZB_ZCL_DOOR_LOCK_SEND_LOCK_DOOR_REQ
ZB_ZCL_DOOR_LOCK_SEND_LOCK_DOOR_REQ(
param,
addr,
ZB_APS_ADDR_MODE_DST_ADDR_ENDP_NOT_PRESENT,
0, // no addr/endpoint needed because using binding
ZB_SWITCH_ENDPOINT, // source endpoint
ZB_FALSE, // no default response
NULL); // command: 0x00 = LOCK, 0x01 = UNLOCK
}
else
{
user_print("send_lock_req %d - not joined or busy\r\n", param);
zb_buf_free(param);
}
}

yongjian