This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2652P: RED certification tests

Other Parts Discussed in Thread: CC2652P

CC2652P device:

we are currently preparing the RED certification process for our electronic device, which integrates your radio module on board.

For the certification tests, the laboratory is requesting a dedicated firmware version for continuous transmission mode, with the following requirements:

  • radio band occupation greater than 98%;
  • operation on the highest radio channel;
  • transmission at maximum output power;
  • availability for both BLE and ZigBee modes.

Could you please confirm whether you already have these firmware versions available and, if so, whether you can provide them to us so that we can load them directly onto the radio module?

Please also let us know if there are any specific instructions, tools, or procedures required for programming the module with these firmware versions and for setting the maximum transmission power.

We remain available for any additional technical information you may need.

BR Luigi