This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I want to run the start_application script (which runs main.bin file) from services on beagle bone black. I am using the Z-Stack_Linux_Gateway-1.0.1. When I run this script through service it increases my CPU utilization for main.bin from less than 1 % ( before running it through service ) to consistently around 80 - 90 % ( after running it through service ) till I stop the service. I am unable to figure out what is the problem and also is it possible to disable the user interface on the Gateway?
I don't have .sevice file. I run "./zigbeeHAgw beaglebone" in one console and "./start_application" in another to start Z-Stack Linux Home GW UI.