Other Parts Discussed in Thread: Z-STACK, CC2530
Hi ALL
there is a PCBA,which supply the WIFI 2.4G signal and there is alway a zigbee coordinator running.
I found that sometimes the ZC boardcast msg alwas being resend as more as 3 times in NWK,
although its ZCL transmit sequence number is same,
and ZED response msg alway need to resend so many times then it could receive the ACK
Q1:
In order to aviod the signal interference issue , could we change the coordinator channel while it is running?
When 2.4G wifi choose the channel 1, change the coordinator channel far from the WIFI channel , such as 25channel !
Q2 :
If above method is OK to implement, How about WIFI bandwidth change as 40Mhz?
because so many people set the WIFI bandwidth as 40MHz, is that work change the ZC channel far from the WIFI channel to avoid
the signal interference issue?
BR!