This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

how to aviod the signal interference issue between WIFI and Zigbee?

Other Parts Discussed in Thread: Z-STACK, CC2530

Hi ALL

         there is a PCBA,which supply the WIFI 2.4G signal and there is alway a zigbee coordinator running. 

         I found that sometimes the ZC boardcast msg alwas being resend as more as 3 times in NWK, 

         although its ZCL transmit sequence number is  same,

         and ZED response msg alway need to resend so many times then it could receive the ACK

 

        

        Q1:

        In order to aviod the signal interference issue , could  we change  the coordinator channel while it is running? 

        When 2.4G wifi choose the channel 1,  change the coordinator channel far from the WIFI channel , such as 25channel  !

         

  Q2 :

     If above method is OK to implement,  How about  WIFI bandwidth change as 40Mhz?

     because so many people set the WIFI bandwidth  as  40MHz, is that work change the ZC channel far from the WIFI channel to avoid

     the signal interference issue?

BR!