This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I am interested in exploring the frequency agility abilities of ZigBee Pro for an application. Thus, I would appreciate a response to the questions from this thread (especially #2 and #3), which I will copy below.
Quote:
(1) Can you confirm that the frequency agility feature is *not* implemented in the ZNP image we're using?
(2) what needs to be changed in the ZNP source to enable this feature prior to IAR re-compile?
(3) at a high level, what are the specification flaws, and what additional management code to use this feature correctly? is this implemented in the ZNP source or on the application processor?
Also, if this feature cannot be utilized with a reasonable amount of development, will it be supported by any updates to the software in the near future?
Thank you for any help you can offer.
-Stephen Kruzick