This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
My understanding is that the ZigBee line is often used with Smart Electrical Meters.
Since it only has a range of 3-400 meters... can the transceivers relay information from the fringes of a Mesh Network, to a central point...
Say, 100 nodes, with 70% of them placed outside the central point...
Say the Smart Meter was the central point...
Can the ZigBee inter-operate with the Smart Meter?
Can the ZigBee transceiver, easily communicate with Wireless Standards: 802.11a, 802.11b/g/n and 802.11ac based modems to report to a central server?
Is it capable of doing this kind of relaying?
Thanks in advance!
Robert
Thank you YiKai,
So if I was providing a product for the Utility Company, I'd be able to grant them access through the Smart Meter and they could control the ZigBee?
And, the products I'm building will be "strung along a distance" for example, there may be 3 within 200m of the Smart meter, then 4 more placed about 400m from the Smart Meter, (with the first three in between) then there could be another group of 4 another 200m distant in that line from the Smart Meter, and another 4 even further away... with the furthest now 800m away from the Smart Meter.
Without using the Internet, will the furthest set of four, be able to use the center set of eight, to reach the three... back to the Smart Meter with two way communication between all 15 units... the data rate is ridiculously slow - on the order of a packet of 256 bytes per minute (or less)?
Your insights are all ready much appreciated!
It'll be great if these ZigBee's will do this!
Best,
Robert