This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I m trying to integrate 3328-Geu 3 series micro motion sensor (zigbee end device) by centalite into my system (bbb+cc2531 as network coordinator).
so when i try to add end device in the network by initiating permit join request from co-coordinator, the end device joins the network but leave immediately.
plz find attached sniffer log for details.
Regards
DC
Is this micro motion sensor based on Zigbee HA profile? I see coordinator sends transport key packet to this micro motion sensor but it seems just restarts. Usually, this is caused by incompatible security settings of Zigbee protocol.
yes, in the datasheet of the product it is mentioned that -
The 3-Series Micro Motion Sensor is fully ZigBee HA
1.2 certified and is guaranteed to function with all
open, ZigBee HA 1.2-certified hubs and devices.
pfa for datasheet of the product DataSheet-3SeriesMicroMotionSensor.pdf
again same issue with Sample Light ZC ,the 3-Series Micro Motion Sensor leave automatically.
on smartrf board lcd display it is displaying Match Desc Req=Non Matched.
pfa for sniffer log-cc2530 as ZC.rar
when i discussed to centralite about this issue-
I m trying to integrate 3328-Geu 3 series micro motion sensor (zigbee end device) by centalite into my system (bbb+cc2531 as network coordinator).
so when i try to add end device in the network by initiating permit join request from co-coordinator, the end device joins the network but leave immediately.
they replied me that -
This usually happens when we do not get a response to the Match Descriptor Request. Does their gateway support IAS (0x0500)?”.
so does linux HA gateway 1.0.1 support " IAS (0x0500) " ?