Other Parts Discussed in Thread: Z-STACK,
Respected All,
I am using CC2530 Chip. i have search some example regarding to CC2530 and i got it from Z-Stack.I am using IAR Workbench for 8051 Evolution copy.
I used SampleLight example and comment some initialization regarding development Board initialization and define input output pin using registers and i add LED blink code.
After that i Download and debug the code step by step, it run perfect and blink LED but while i stop debugging, it also stop blinking in cc2530 Chip.
Can anyone help me how to get start with CC2530 Chip?
Sample code is here,
static void delay(unsigned int _dly );
P0SEL |= 0x00 ; //General Purpose I/O
P0DIR |= 0xFF ; //Make Port 0 as Output
HalLedInit();
while(1)
{
HalLedSet(HAL_LED_ALL,1);
delay(500);
HalLedSet(HAL_LED_ALL,0);
delay(500);
}
I have attached images regarding my hardware setup.
Thanks,
Darshit