Hi Ti
I have two CC2530 development kit and I write a simple RF code to transmit numbers from ( 0 to 254 ) from one kit to another and show them using UART0 .
now i want to use each kit as transmitter and receiver.
this mean that i want to send data from kit 1 to kit 2 and then transmit data from kit 2 to kit 1 how can i do this ?
how can i adjust the receive time and transmit time for Two kits So that there is no overlap to the data?
this is the transmitter code
this is the receiver code