This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2538: CC2538 high frequency emission test

Part Number: CC2538

Dear Alex,

We are using the cc2538 per test firmware to do the high frequency emission test. The CC2538 is at 2475MHz Rx mode. The test is failed as shown in the attached document. It is surprised that there is no fundamental frequency 2475 MHz, but the second harmonic 4950 MHz present. Please comments. Besides, please tell us where are the 3222.659375MHz and 3256.000000MHz  tone come from

17120501HKG-001 socket outlet - zigbee Rx above 1G.pdf