Part Number: CC2531
Other Parts Discussed in Thread: Z-STACK
I've been working with making CC-2531 work as ZigBee for my Final Year Project. So far I've been able to create a network and send (or broadcast) data (in decimal) and receive on the receiver side in hex format with the help from TI community. I have 2 questions from the experts, which are as follows:
1) Can I send file(s) (doc, audio, video) from one to another CC-2531? If yes, would it require writing a code or it can be done directly from the Z-Tool?
2) What's the possibility of changing the security in the stack? For example, can I change the S-boxes in the z-stack and then use it with CC-2531?
I am in real need of help and any of it from TI community will be highly appreciated.
Many Thanks,
- Arslan