This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I've been trying to use Z-Tool to create a network and have searched a lot on the internet but haven't understood the way to do so. I have also worked very hard to understand Z-Tool Monitor and Test guide.
I have three CC2531 dongles with z-stack burned onto them. I want to create one of these as a coordinator while the other two as end devices. How to change the device type? As you can see, there is "None" written in the screenshot at present.
After that, I wish to send messages between these. Which commands from the z-tool shall I use to send messages? The guide doesn't explain parameters with examples, so it's getting really confusing.
If anyone can guide me through the process, it will be highly appreciated.
Looking forward to your help
Thank you!
Thanks for your reply, YiKai. The screenshot can be seen at the top of this thread, just above the first message.
For instance, I make one zigbee as a coordinator while the other two as end devices. As soon as I do so, the end devices will automatically join the network, is that right?
Then I should be able to broadcast a message from the coordinator to all nodes in the network. Which command do I use for this purpose?
Looking forward to your response
Thanks
Hey YiKai,
Just as you suggested, after I configured coordinator I configured end device within 180s, but the router didn't join the network which I observed when looked at associated devices where nothing was showing up. Also, here's what shows when completed the commissioning commands and the announce is run
<TX>11:45:19.67 COM10 ZDO_END_DEVICE_ANNCE (0x250A)
NwkAddr: 0x0000
IEEEAddr: 0x0000000000000000
Capabilities: NONE (0x0)
Moreover coordinator and router configured in separate PCs have the same short address i-e 0x0000. Do you think of it as an issue?
Please suggest an alternate measure to configure devices correctly so they can join coordinator automatically.
Thanks
Hi,
By "download ZNP", do you mean reflash with Z-Stack or just plug into the port and write the commands again?
If latter is what you mean, then I've tried it many time by doing a hard reset. However, in the end the router doesn't join the network.
Waiting for your response