This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello, everyone. I have a problem as following. I have several coordinators and want each of them to connect only with specified 4 end devices.
Say, I want coordinator A to connect only with specified 4 end devices 1,2,3,4 and coordinator B to connect only end devices 5,6,7,8.
the firmware of A and B is the same and the firmware of end deivce1 to 8 is the same.
let's suppose end device 5 try to join coordinator A instead of B.
in case like this, I use function "NLME_LeaveReq" to make end device 5 leave the network created by coordinator A.
Generally, this scheme works well. But the matter is, when I restart coordinator(s) or end devices, some end devices(which is previously connected) doesn't connect with the coordinator which it's supposed to connect.
(for example, after restarting coordinator A, the end device 3 doesn't connect with coordinator A. even if the end device is connected, it takes a lot of time.)
please help me.
Thanks.