Other Parts Discussed in Thread: CC2530, Z-STACK, UNIFLASH, CC2652R, CC2530EMK
Hi TI team
I can not ota end device(CC2538 as server,dongle CC2530 as a client.)
ZC:CC2538(ota_dongle) ZED:CC2530/CC2538 PDF:Z-Stack OTA Upgrade User's Guide channel:25 panid:0x2222(modify Configuration file)
The CC2538 Board :1.update the D:\Texas Instruments\Z-Stack 3.0.2\Projects\zstack\OTA\Dongle\CC2538
2.modify add source code on the Dongle:void OTA_Dongle_Init( byte task_id )
{
osal_start_timerEx( OTA_Dongle_TaskID, OTA_DONGLE_DONGLE_5S_EVT, 5000 );
bdb_StartCommissioning(BDB_COMMISSIONING_MODE_NWK_STEERING|BDB_COMMISSIONING_MODE_NWK_FORMATION | BDB_COMMISSIONING_MODE_FINDING_BINDING | BDB_COMMISSIONING_MODE_INITIATOR_TL);
}
3.add function: every 5s open the network and enable the CC2592.
The CC2530 Board:1.update the Boot D:\Texas Instruments\Z-Stack 3.0.2\Projects\zstack\OTA\Boot\CC2530DB
2. modify source code:void zclSampleSw_Init( byte task_id )
{
bdb_StartCommissioning(BDB_COMMISSIONING_MODE_NWK_STEERING| BDB_COMMISSIONING_MODE_FINDING_BINDING);
}
3. config the sample switch application example, update the EndDeviceEB-OTAClient
4.had generated the image:5678-1234-00000001.zigbee.
result:1 .it can not join the CC2538,2 had no find any can update CC2530 firmware from the otaserver tools.
The CC2530 Board:1. modify source code:void zclSampleSw_Init( byte task_id )
{
bdb_StartCommissioning(BDB_COMMISSIONING_MODE_NWK_STEERING| BDB_COMMISSIONING_MODE_FINDING_BINDING);
}
2.config the sample switch application example, update the EndDeviceEB.
result: 1.it can join the CC2538.
3.from the picture,i can not learn about update firmware any information,
4.from the wireshark packet had no any response
5.But the CC2538 as a client is successfully update.
So I had any operation error about CC2530 as a client?
Thanks!