This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2531EMK: cc2531

Part Number: CC2531EMK
Other Parts Discussed in Thread: CC2531, , CC2540

was there any real resolution discovered?' Im having the same issue.... cc2531 not showing  up at all in windows, but flashes fine etc....... only thing i would like to add is that windows does make the sound when i plug it in like it recognises it but nothing, and the green light is on at first but then goes off after abit.