This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP-CC2652RB: Smart RF Sniffer won't detect my device

Part Number: LP-CC2652RB
Other Parts Discussed in Thread: UNIFLASH, FLASH-PROGRAMMER, PACKET-SNIFFER

I've gone through the setup instructions listed in the SmartRF Packet Sniffer 2 User Guide several times.

I cannot seem to get the Packet Sniffer application to detect my LP-CC2652RB with sniffer firmware installed.

I am using a microcontroller with Rev E silicon.

One note when looking through the forums, I read someone had resolved this same issue on a CC26x2R1 by setting the serial port baud rate to 921600.

I already had that setting selected, however there are not any COM ports to choose from in the settings.

COM14 and COM15 are the ports that populate in my Device Manager for the XDS110 debugger and application.

What should I do next?

Thanks,

Anthony