Part Number: CC2530
Hello there!
I noticed that, after sending a couple of broadcast mensages correctly to all routers and coordinator, sundely, only the parent starts to receive the same broadcast msg.
With the packetSniffer I've check out that the two first bytes from MAC Payload, changed from 08 02 to 08 22. Is it related to security options? Why this change?
In the attached file, the address 0xA82B is my ZED, which is sending broadcast. You can observe that, after a power cycle, this device does an Beacon Request, then broadcast a mensage. The first message goes well, but in the next msg only the parent receive the broadcast.
Below is a picture of this the MAC Payload difference.
By the way, I've attached the sniifer file.