Part Number: CC2652P
When a Device join into a Network, ZDP Device Announce command will be broadcasted to all over the Network. It is an important message for Network Manager Device.
But when many device are joining into a Network, broadcast message will be sent failed easily. So the Application layer should have chance to retry to send ZDP Device Announce command.
void (*pZdoAnnounceNewAddrFailureCB)(uint8_t status) = NULL;
/*********************************************************************
* @fn ZDApp_AnnounceNewAddress()
*
* @brief Send Device Announce and hold all transmissions for
* new address timeout.
*
* @param none
*
* @return none
*/
void ZDApp_AnnounceNewAddress( void )
{
// Turn off data request hold
APSME_HoldDataRequests( 0 );
// new function to send ZDP Device Announce with AF confirm callback
afStatus_t status = ZDP_DeviceAnnceEx( NLME_GetShortAddr(), NLME_GetExtAddr(),
ZDO_Config_Node_Descriptor.CapabilityFlags, 0, ZDO_AnnounceNewAddrConfirmCB, NULL );
// Trigger callback when Device Announce sent failed, add by luoyiming 2021-05-08
if( status != ZSuccess && pZdoAnnounceNewAddrFailureCB )
{
pZdoAnnounceNewAddrFailureCB( status );
}
// Setup the timeout
APSME_HoldDataRequests( ZDAPP_HOLD_DATA_REQUESTS_TIMEOUT );
if ( ZSTACK_END_DEVICE_BUILD )
{
if ( zgChildAgingEnable == TRUE )
{
uint8_t coordExtAddr[Z_EXTADDR_LEN];
// Send the message to parent
NLME_GetCoordExtAddr( coordExtAddr );
NLME_SendEndDevTimeoutReq( NLME_GetCoordShortAddr(), coordExtAddr,
zgEndDeviceTimeoutValue,
zgEndDeviceConfiguration );
}
}
}
/*********************************************************************
* @fn ZDO_AnnounceNewAddrConfirmCB
*
* @brief Send Device Announce confirm callback
*
* @param same with pfnAfCnfCB in af.h
*
* @return none
*/
void ZDO_AnnounceNewAddrConfirmCB( uint8_t status, uint8_t endpoint, uint8_t transID, uint16_t clusterID, void* cnfParam )
{
// Trigger callback when Device Announce sent failed, add by luoyiming 2021-05-08
if( status != ZSuccess && pZdoAnnounceNewAddrFailureCB )
{
pZdoAnnounceNewAddrFailureCB( status );
}
}