This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello TI,
What’s the minimum needed to program a CC2650? I don’t think the sensor kit is adequate for my needs.
Would it be the SimpleLink CC2650 EVM + the SmartRF Flash Programmer 2 SW?
Thanks,
Dan
Hello all,
I will work on CC2650STK. So should we understand that the CC2650DK is the least to start programming and debugging this kit. Or IAR / Smart Flash Programmer 2 and JTAG emulator (XDS100 for instance) would be enough for our purposes?
Regards
Tunç
Q: Which debuggers are supported?
A:
I don't have a XDS200, but I guess it will work with a few setting changes.
Hi guys,
i will add my question to discution to not duble the topics.
I can see that both cc2650 and cc2640 have cjtag and on pinout there are 4 pins for standard jtag. on wiki i can see http://processors.wiki.ti.com/index.php/CC13xx_CC26xx_Tools_Overview
that it is possible to use segger j-link debugger. Can you 100% confirm me that ?
Hello,
I reproduced the tida-00374 board but when I try to program the CC2650 installed there by smartrf06 and flash programmer, the chip is recognized but the flash size results 0k and the programming fails (as well as flash reading). I checked the debug interface (cjtag) harware and everything seems to be ok: can you help me?
Can Tida - 00374 board be purchased?