Hello,
I'm trying to adjust the I2C registers on my TPA0172 amplifier, however when I read from the I2C
bus, it appears to never complete the power up sequence. Bit 7 of register 5 (mask register)
never goes to 0. I read this information from the bus. READ Register 1 3F Register 2 3F Register 3 3F Register 4 3F Register 5 FF Register 6 0 Which is all correct for the power up values of this amplifier, but register 5 should change to 7F
when it's done powering up, according to my understanding from the data sheets. Then I
should be able to write to it. Any ideas?
Currently running
2.2k pull up resistors on SDA, SCL
I2CVdd = 5v
The master device is an mbed uC and the TPA0172 is the only slave on the bus.
Thanks for the help. Ryan