Hello,
I have a question regarding the grounding & thermal interface of the heat slug & heatsink.
I one of the several posts about the TASS5630B, a TI engineer replied, saying that proper grounding of the heatsink is important because currents flow directly rfom the heat slug into the heatsink. If not grounded properly (impedance/inductance), the chip can get confused.
The datasheet of the TAS5630B says:
(1) Achievable output power levels are dependent on the thermal
configuration of the target application. A high-performance
thermal interface material between the exposed package heat
slug and the heat sink should be used to achieve high output power levels.
Most of the thermal interface materials available (greas, films) are NON conductive.
And even if they are conductive, the impedance will never be that low as in mili-ohms, so high swithcing currents can flow freely...
Are there some kind of thin copper foils maybe, that will do both jobs; compensating/filling the roughness of the heat slug & heatsink and thermal conductiviness?
Kind regards,
Benjamin Hoogendoorn
Designing a mono-aplifier with the TAS5630b DKD in PBTL for active subwoofer application