Hello Sir,
I am using LM4780 IC of single channel to get 60W RMS Output from each channel.I am using ckt of Fig.39 of LM4780 datasheet to check on General purpose PCB.In that there are two high pass filter ckts (RIN1,CIN1) and (Ri1,Ci1).By claculating those values I got the cutoff frequency as 10.6Hz and 2.3Hz respectively.
I need to drive the Output of LM4780 to a 100V Audio Step-up transformer instead of loudspeaker.To eliminate the core saturation of the transformer at low frequecny response,we have to set the high pass filter at the input of Power amplifier from 80Hz to 120Hz.I need to set to 100Hz.
Please suggest where to change the values of RC combination to set the high pass filter from Fig.39 (Pg.No 24) of LM4780 datasheet (either RIN1,CIN1 or Ri1,Ci1).?
With Regards,
Suneetha.V