Hi Sir
TAS5754 support 3-Wire Digital Audio Interface ( No MCLK required). How did we use this function?
Did we need setting FW or HW?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sir
TAS5754 support 3-Wire Digital Audio Interface ( No MCLK required). How did we use this function?
Did we need setting FW or HW?
Hi Kerr,
It's done via PLL register settings in the datasheet. Below is a example I2C for 3-wires that can get you started.
!3wire mode !System Clock PLL mode with NO SCLK input mode. Provide supply voltages(3.3V). Don't provide I2S clocks yet. ! Write 0x00 at address=0x00 via I2C. (Go to page.0) X00 00 ! Write 0x10 at address=0x02 via I2C. (Standby request) X02 10 ! Write 0x5A at address=0x25 via I2C. (Ignore SCLK hault detector, Ignore SCLK detection, disable auto divider settings, ignore fs detection) X25 5A ! Write 0x10 at address=0x0D via I2C. (PLL clock source => BCLK) X0D 10 ! Write 0x00 at address=0x14 via I2C. (P=1 for PLL divider) X14 00 ! Write (0x10 for BCLK=64fs, 0x20 for BCLK=32fs note that L&R 32 bit = 32*2=64) at address=0x15 via I2C. (J=16/32 for PLL divider) X15 10 ! Write 0x00 at address=0x16 via I2C. (D1=0 for PLL divider) X16 00 ! Write 0x00 at address=0x17 via I2C. (D2=0 for PLL divider) X17 00 ! Write 0x01 at address=0x18 via I2C. (R=2 for PLL divider) X18 01 ! Write 0x01 at address=0x1B via I2C. (miniDSP CLK divider = 2) X1B 01 ! Write 0x0F at address=0x1C via I2C. (DAC CLK divider = 16) X1C 0F ! Write 0x03 at address=0x1D via I2C. (NCP CLK divider = 4) X1D 03 ! Write 0x07 at address=0x1E via I2C. (OSR CLK divider = 8) X1E 07 ! Write 0x00 at address=0x22 via I2C. (Interpolation filter = 8x, fs setting = 48kHz) X22 00 ! Write 0x04 at address=0x23 via I2C. (IDAC = 1024 cycles) X23 04 ! Write 0x00 at address=0x24 via I2C. (IDAC = 1024 cycles) X24 00 ! Write 0x00 at address=0x02 via I2C. (Standby release) X02 00 ! Provide I2S clocks (SCLK : Tie to 0, LRCLK : 44.1kHz/48kHz, BCLK : 32fs/64fs)
reg,
Paul Chen.
Audio Apps.