Our customer has questions about TPA2000D1.
I'm posting the questions for a customer:
++++++++++++++++++++++++++++++++++++++++++++++
We are evaluating a TPA2000D1 with a ferrite filter for a speaker output.
The filter is adopted because there was noise by the previous model.
To have the noise radiated from the speaker wire, we're in trouble.
The ground line of the filter capacitor receives a noise.
A frequency of the noise is 480MHz that relates to CPU/SDRAM clock
frequency:120MHz.
The noise is radiated from the speaker wire.
(The length of the wire is 5 inches.)
Questions;
(1)
We're considering to eliminate the filter capacitors only and to leave the
beads.
Are there any problems?
(2)
How much is the maximum current value which flows to beads?
(When choosing beads, we refer to the value.)
++++++++++++++++++++++++++++++++++++++++++++++
Thanks in advance.
Takishin